AND, OR, and XOR
You can use AND, OR and XOR for multiple conditions. These keywords provide the following results:
Input Values | AND | OR | XOR |
---|---|---|---|
Input A = True Input B = True |
True |
True |
False |
Input A = True Input B = False |
False |
True |
True |
Input A = False Input B = True |
False |
True |
True |
Input A = False Input B = False |
False |
False |
False |
The syntax for entering an AND, OR or XOR keyword is:
<Value-name> := <Value1> <Keyword> <Value2>;
where <value-name>
is the name of the variable that will store the result of the statement, <Value1>
is the first input value, <Value2>
is the second input value, and Keyword is AND, OR or XOR as required.
Example:
Output := Input1 AND Input2;
This sets the value of the variable named Output to be True if Input1 and Input 2 are both True, or False if only one of the inputs is True.
Output := Input1 OR Input2;
This sets the value of the variable named Output to be True if either Input1 or Input 2 are True. The Output value will only be False if both of the inputs are False.
Output := Input1 XOR Input2;
This sets the value of the variable named Output to be True if one of the inputs is True and the other is False. The Output will be False if both of the inputs are True or if both of the inputs are False.