Define the Execution Settings for a Logic Program

When you have defined the program code for your program, you need to configure it so that the system can execute it. To do this, you need to use the various Execution settings, the Trigger setting and the Execution Queue Size setting. Depending on your selections, the system will execute the program:

To define the execution settings for a Logic Program:

  1. Display the configuration Form for the relevant program (see Configure an ST Program, Ladder Diagram, SFC or FBD).
  2. Select the Logic tab.
  3. Define the following execution-related settings:
  4. Save the configuration changes you have made.

Disclaimer

Geo SCADA Expert 2019