Function Block Diagram Components

Function Block Diagrams can consist of the following items:

The various components of a Function Block Diagram are connected via connection lines, which you can draw to link the connection box of one component to a connection box on another component. These connections allow you to control the flow of the Function Block Diagram (see Edit a Variable on a Function Block Diagram).


Disclaimer

Geo SCADA Expert 2019