Operators

Operators are the calculations and conditions that are used to define the behavior that is provided by a Logic program. Each operator provides a specific calculation or comparison, for example, the > operator means 'greater than' and the < operator means 'less than'. They can be used in an expression that compares values like this:

IF Value1 > 50 THEN

Value2 := 10;

ELSIF Value1 < 50 THEN

Value2 := 5;

END_IF;

In this expression, if Value1 is greater than 50, then Value2 is 10. If Value1 is less than 50, then Value2 is 5.

Each operator has a precedence level. This determines the order in which the operations are evaluated.

The following table shows the available operators and their precedence:

Operator Description Precedence Level

( <expression> )

Expression inside parentheses ( )

1 (Highest)

Function (<expression>)

Parameter list of a function or function evaluation

2

**

Exponentiation

3

-

Negation

4

NOT

Value with opposite sign

4

*

Multiplication

5

/

Division

5

MOD

Modulus operation

5

+

Addition

6

-

Subtraction

6

<

Less than

7

>

Greater than

7

<=

Less than or equal to

7

>=

Greater than or equal to

7

=

Equality

8

<>

Inequality

8

AND, &

Boolean AND

9

XOR

Boolean exclusive OR

10

OR

Boolean OR

11 (Lowest)


Disclaimer

Geo SCADA Expert 2019