RIGHT

Function Name

RIGHT

Description

Outputs a specific number of characters taken from a string input. The characters are taken from the right-hand side of the input string (ending with the last character).

Arguments

IN {STRING}

The IN input is a string input. The RIGHT function uses characters from the IN input for its output.

L {INT}

Defines the number of characters in the IN input that are used for the output. The output ends with the last character of the IN input and starts the L number of characters prior to the end.

For more information on the data types for the inputs and outputs, see Data Type Hierarchy.

Returns

Output {STRING}

The output is a string that is the L number of characters from the IN string, starting from the right.

Example:

Function Block Diagram - RIGHT:

In this example, the IN input is 'PIPELINE STRUCTURE FAILURE' and the L input is 17. This means that the RIGHT function will return 17 characters from the IN input, starting with the right-most character (the last character). So, as the IN input is 'PIPELINE STRUCTURE FAILURE', the RIGHT function outputs 'STRUCTURE FAILURE' (the last 17 characters from the IN string).

ST Program - RIGHT:

To use a RIGHT function in an ST program, you need to use this syntax:

Output := RIGHT ('IN', L);

Where Output, IN and L are defined as variables earlier in the ST program.

Alternatively, you can use the following syntax:

Output := RIGHT (IN:= 'PIPELINE STRUCTURE FAILURE', L:= 17);

Where the 'PIPELINE STRUCTURE FAILURE' and 17 values are the input values (in this case, they are the same values as used in the Function Block Diagram example above).


Disclaimer

Geo SCADA Expert 2019