SUB_DT_TIME

Function Name

SUB_DT_TIME

Description

Subtracts a time input from a date time input to provide a date time output.

Arguments

Input 1 {DATE_AND_TIME}

Input 2 {TIME}

For more information on the data types for the inputs and outputs, see Data Type Hierarchy.

Returns

Output {DATE_AND_TIME}

The Output is the result of Input 1 - Input 2

Example:

Function Block Diagram - SUB_DT_TIME:

A SUB_DT_TIME function has 2 inputs (in this case, a NOW function and a constant):

  • Input 1 is connected to a NOW function
  • Input 2 is set to T#45m.

The SUB_DT_TIME function returns a date time value that is the result of the current date and time - 45 minutes.

ST Program - SUB_DT_TIME:

The syntax for a SUB_DT_TIME function in an ST Program is:

Output := SUB_DT_TIME (Input 1, Input 2)

Where Output, Input 1 and Input 2 are defined as variables earlier in the ST program. Input 1 is a date time value, Input 2 is a time value, and the Output is a date and time value.


Disclaimer

Geo SCADA Expert 2019