Sequential Function Charts
            Sequential Function Charts represent a sequence of Logic. They allow you to create a Logic program that defines system behavior that occurs in steps, depending on specified conditions.
One of the main advantages of Sequential Function Charts (SFCs) is that only the active parts of the SFCs are executed, and you can easily see which parts are inactive. This means it is easy to determine what condition caused a step to occur.
The following sections explain the basic concepts of Sequential Function Charts and explain how to set up an SFC. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.
For information on the properties of the Sequential Function Chart database items, see Logic Program Properties and Values.