Timers

The timer function blocks are useful when you need an output to be dependent on the state of an input, but also require a delay. Delays with state changes are often needed when the communications equipment is known to be unreliable, for example, when you know that sensors sometimes report incorrect states due to signal interference.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

Geo SCADA Expert 2019