UTC_TO_LOCAL

Function Name

UTC_TO_LOCAL

Description

Outputs the time provided by Input 1 in Local time format. This allows the ST program to make adjustments according to local time changes such as British Summer Time.

Local time settings are defined by the operating system.

Arguments

Input 1 {DATE_AND_TIME - UTC time format}

For more information on the data types for the inputs and outputs, see Data Type Hierarchy.

Returns

Output {DATE_AND_TIME - Local time format}

Function Block Diagram - UTC_TO_LOCAL:

The UTC_TO_LOCAL function converts a date and time input from Coordinated Universal Time into local time. In the example shown above, the UTC_TO_LOCAL function applies the local time settings to the input time and date. In this case, the UTC_TO_LOCAL function takes the input time and adds 1 hour for the output (the local time settings are 1 hour in advance).

ST Program - UTC_TO_LOCAL:

The syntax for a UTC_TO_LOCAL function in an ST Program is:

Output := UTC_TO_LOCAL (Input 1);

Where Output and Input 1 are defined as variables earlier in the ST program. The Input 1 variable represents a Date and Time value.

Further Information

Time Zones: see Time Zone Support in Geo SCADA Expert in the Geo SCADA Expert Guide to Core Configuration.


Disclaimer

Geo SCADA Expert 2019