Configuring Lufkin SAMS Controllers

The Lufkin SAMS driver is designed to allow Geo SCADA Expert to interface with the SAM series of Lufkin rod pump controllers. The controllers are represented by outstation items in the Geo SCADA Expert database.

The Lufkin SAMS driver supports these types of controller (outstation):

If your database structure is ‘modular’ and Group Templates are used to store ‘model’ Lufkin SAMS configuration, in addition to the above types of controller, you can add this driver-specific ‘abstract’ controller item to your Group Templates:

You can only add Abstract Items to Group Templates. The abstract items appear as additional driver-specific entries when you display the context sensitive menu from a Group Template. As with other abstract items, in order to represent a ‘real’ controller, you need to convert the abstract items into the required type of controller (outstation) within the Group Instances that reference the Group Template. For more information, see Add an Abstract Item to a Group Template in the Geo SCADA Expert Guide to Core Configuration.

You specify each controller’s properties using the fields on the appropriate Lufkin SAMS Outstation Form.

Each Lufkin SAMS Outstation Form has several tabs.

Use the Lufkin SAMS tab to:

For information on the other tabs, see Configuring a Generic Modbus Controller in the Geo SCADA Expert Guide to the Advanced Modbus Driver.

For information on the minimal amount of configuration that you can undertake to produce a functional Lufkin SAMS controller in Geo SCADA Expert, see Minimum Configuration.


Disclaimer

Geo SCADA Expert 2019