Upload Event Log

Associated with: Lufkin SAMS controllers

Security permission required to access this pick action: Retrieve Data

Use the Upload Event Log pick action to upload to Geo SCADA Expert the entries that are stored in the controller’s Event Log. The pick action enables Geo SCADA Expert to upload multiple events at a time, should more than one event exist in the controller’s Event Log at the time that the pick action is triggered. Geo SCADA Expert stores the controller’s events in the Event Journal. Each controller event:

The controller’s Last Outstation Event status attribute provides information about the latest controller event that Geo SCADA Expert has uploaded (see Lufkin SAMS Controller Status Attributes).

NOTE: If using this pick action with the Automation Interface, you need to specify the method name UploadEventLog.


Disclaimer

Geo SCADA Expert 2019