Alarm Limits

Use the fields within the Alarm Limits section of the Counter Point tab to set limits for an MQTT JSON Schema A counter point and specify whether an alarm or event is generated if the point exceeds those limits.

For information on configuring Alarm Limits properties, including the Alarm Limits fields that are common to many counter-type points, see Configure the Limits for a Counter-Type Point in the Geo SCADA Expert Guide to Core Point Configuration.

For information on the Tune Limits feature, see Define Whether a Counter-Type Point’s Limits can be Tuned in the Geo SCADA Expert Guide to Core Point Configuration.

If the Area of Interest feature is enabled on your system, an Area of Interest field is displayed within the Alarm Limits section. For more information on this property, see Specify the Area of Interest Associated with a Point’s State-Related Alarms and Events in the Geo SCADA Expert Guide to Core Point Core Point Configuration.


Disclaimer

Geo SCADA Expert 2019