Configure the Point Scaling

Use the fields within the Scaling section of the Analog Point tab to configure a point's scaling. The MQTT JSON Schema A driver applies the scaling to each value that it retrieves from the device, before passing the resultant value to the Geo SCADA Expert database.

The Raw Scale properties in the Scaling section enable you to optionally scale the range of raw input signals into a range of floating-point engineering values for use in the Geo SCADA Expert database.

The Multiplier and Offset properties enable you to adjust the floating-point engineering values to align them with other values in your database.

Use these fields to configured the required scaling:


Disclaimer

Geo SCADA Expert 2019