About Geo SCADA Expert Maps

You can create single-layer maps or multi-layer composite maps in Geo SCADA Expert, from online or offline mapping sources, which you can then use for a variety of purposes. For example, you can display:

Geo SCADA Expert maps have one or more layers. There are two types of map layer, as follows:

In Geo SCADA Expert, you can display a base layer map as a standalone map (for example, to use as a framework to display the location of a database item) or you can create maps which have a base layer and one or more overlays. You can also create maps which offer a user a choice of base layer and a choice of overlays to display.

For example, a base layer map could be a map of Europe, which might look like this:

You could either display this map as a standalone map or you could overlay this base layer map with rainfall data, as follows:

To create a map, you need to specify which layers will make up your map, and specify the sources of these layers (these can be online or offline sources). For more information, see Creating a Geo SCADA Expert Map.

Once you have created a map, you can then display it in Geo SCADA Expert (see Displaying a Geo SCADA Expert Map).

When users display Geo SCADA Expert maps, they can zoom in and out to see more or less detail. Users may also have a choice of base and overlay layers to view (see Using a Geo SCADA Expert Map).


Disclaimer

Geo SCADA Expert 2019