Add a Custom Pick Action Menu

To add a custom pick action menu:

  1. Display the Pick Menu window (see Using the Pick Menu Window).
  2. Select the Add Menu button.
    A new menu is added to the pick action menu tree structure. It is selected automatically, ready for you to define its name.

  3. Enter a suitable name, then press the Enter key or select another part of the interface to confirm the name entry.

When you have added a menu, you can add pick actions to the menu (see Add a Custom Pick Action) and move the menu in the pick action menu tree structure (see Change the Order of Custom Pick Actions, Menus, and Separator Lines).


Disclaimer

Geo SCADA Expert 2019