Creating a View

To create a View:

  1. Display the Mimic that contains the area to be included in the View. You need to display the Mimic in Design mode (see Displaying a Mimic).
  2. Use the magnification tools to zoom in on the area that is to be shown in the View (see Magnifying a Mimic (Zooming)).
  3. Select the Graphics tab on the ViewX ribbon.
  4. Select Views in the View command group.

    The Views window is displayed.

  5. Select the Add button to add a new View to the list. The View is selected automatically, ready for you to define its name. The View already has the X, Y, W, and H settings (X and Y coordinates for the section of the Mimic and width and height settings for the size of the View) for the area of the Mimic that you magnified in step 2.
  6. Enter a suitable name for the View, then press the Enter key or select another part of the interface to confirm the selection.
  7. Select the Close button.
  8. Repeat this procedure for each View that you require.

You can change the View settings by using the Edit feature (see Editing a View).

Only users with the Configure permission can create Views.


Disclaimer

Geo SCADA Expert 2019