Enable or Disable Anti-Aliasing for New Mimics on your Client PC

You can use the Mimic Properties window to enable or disable the Anti-Aliasing feature on new Mimics by default. To do this, you specify your requirements using the Mimic Properties window that you access via the Options window. The Anti-Alias setting applies to new Mimics that are displayed on your client PC and are being configured for the first time. New Mimics that are being displayed and configured on other client PCs are unaffected by your selections.

For the Anti-Aliasing feature to be applied to new Mimics, it has to be enabled for Mimics (see below) and also enabled on your client PC (see Enable or Disable Anti-Aliasing for your Client PC).

To enable or disable Anti-Aliasing for new Mimics, you have to access the Mimic Properties window via the Options window:

  1. Display the Options window.
  2. Select the Mimics tab.
  3. On the Mimics tab, select the Edit button in the General section.
    The Mimic Properties window is displayed.
  4. On the Mimic tab of the Mimic Properties window, use the Anti-Alias check box to define whether Anti-Aliasing is enabled or disabled on any new Mimics displayed on your client PC:
    • Select the check box to enable the Anti-Aliasing feature by default on new Mimics (on your client PC only)
    • Clear the check box to disable the Anti-Aliasing feature by default on new Mimics (on your client PC only).
  5. Close the Mimic Properties window.
  6. Select the OK button to confirm your selection and close the Options window.

If you access the Mimic Properties window by using the Properties option or command on a Mimic, the changes you make will only apply to that specific Mimic. You have to access the Mimic Properties window via the Options window to apply settings that are applied to each new Mimic by default.


Disclaimer

Geo SCADA Expert 2019