FlashAlpha

The FlashAlpha property defines the amount of transparency for the flash color that is used in a flash effect for the outline or line. This works in exactly the same way as the FlashFillAlpha property in the Fill group of properties except that it applies to the line instead. For more information, refer to FlashFillAlpha.


Disclaimer

Geo SCADA Expert 2019