FlashFillColour

The FlashFillColour property defines the alternate FillColour that is used with a flash effect. When animated to use the flash feature, the object will alternate between the FillColour and the FlashFillColour.

The FlashFillColour works in exactly the same way as the FillColour except that it corresponds to the alternate color for flash effects.


Disclaimer

Geo SCADA Expert 2019