General Tab (Embedded Query List)

The General tab for embedded lists contains several settings that are common to General tabs, including Name, Visible, Animations, Pick Action, ToolTip, and the Dynamic Position settings. For more information on these common settings, see General Tab.

The General tab for embedded Lists also contains settings that are specific to embedded Lists. You can use these specific embedded List settings to:

The settings that are specific to embedded Lists on Mimics are:


Disclaimer

Geo SCADA Expert 2019