Moving the Mimic within the Display (Panning)

You can use the Pan tool to move a Mimic within the ViewX Document Display Area or Virtual ViewX Document Display Area. This is useful when you want to look at another part of a Mimic without changing the level of magnification.

To pan a Mimic:

  1. Activate the Pan tool:

    In ViewX, select Pan Mode in the Navigation command group on the Home tab.

    In Virtual ViewX, right-click on the background of the Mimic to display a context sensitive menu, then select the Pan option.

  2. Select any area on the Mimic and keep the left-hand mouse button pressed down.
  3. Move the cursor to move the Mimic within the ViewX Document Display Area.
  4. Release the left-hand mouse button when the required part of the Mimic is shown.

Disclaimer

Geo SCADA Expert 2019