Understanding the Animation Properties

The animation properties that are shown in the Animations window vary according to the type of object you are trying to configure. If you are trying to configure an animation for a Mimic object and need more information about a particular animation property, please refer to the relevant section:

For information on the various features of the Animations window, see Using the Animations Window.


Disclaimer

Geo SCADA Expert 2019