Use Drag and Drop to Create a New Text Box Hyperlink

To use drag and drop functionality to create a hyperlink in a new text box:

  1. Display the Mimic that is to contain the new hyperlink. You need to display the Mimic in Design mode (see Displaying a Mimic).
  2. Either:
    1. In ViewX, use the Database Bar to locate the item that is the 'target' of the hyperlink. The 'target' display will be:
      • The graphical display for any item that is configured graphically, such as Pre-Configured Trends, X-Y Plots, Schedules, Mimics, Function Block Diagrams and so on.
      • The configuration Form for any database item that is not configured graphically, for example, database points, channels and outstations.
    2. Select the item and keep the left-hand mouse button pressed down. Proceed to step 3.

    Or:

    1. Use Windows Explorer to locate the file that is the 'target' display.
    2. Size the Windows Explorer window and the ViewX window so that you can drag the file icon from the Windows Explorer window onto the Mimic.
    3. Select the icon for the file. Keep the left-hand mouse button pressed down. Proceed to step 3.

    Or:

    1. Use a supported web browser to display the web page that is to be the 'target' display.

      Remember that if your system uses Original WebX clients, those clients have to use the 32-bit version of Internet Explorer. Other browsers are not supported.

    2. Size the browser window and the ViewX window so that you can drag the file icon from the Address field on the browser onto the Mimic.
    3. Select the icon for the web page (in the browser's Address field). Keep the left-hand mouse button pressed down. Proceed to step 3.
  3. Drag the item onto the Mimic's design area, then release the left-hand mouse button.
    A context sensitive menu is displayed.
  4. Select the Hyperlink option.
    A new text box is added to the Mimic. It is automatically configured to act as a hyperlink to the display you selected in step 2.

You can alter the text in the text box and change its appearance in the same way as you would edit any other text box (see Editing a Text Box). You can also edit the animations that are in place for the hyperlink (see Text Box Animations). If you want to change the ToolTip for the hyperlink or set the 'target' display to be shown in a new window, use the Pick Action Configuration Wizard (see Using the Pick Action Wizard to Create a Hyperlink).

When the Mimic is displayed in Run mode, users will be able to select the hyperlink text box—when it is selected, the relevant 'target' display will be shown.


Disclaimer

Geo SCADA Expert 2019