Using the Options Window to Define Settings that apply to All Mimics

You can use the Options window’s Mimics tab to define settings that apply to:

To display the Options Windows, see ViewX Options.

The settings that you apply for Mimics via the Options window are specific to your client PC, and they allow you to define:

The settings you apply via the Options window’s Mimics tab apply to those Mimics that are displayed or created on your client PC only. When the same Mimics are displayed on other client PCs, different settings may be applied (depending on the Options settings on the other clients).

Be aware that the Mimic Properties window that you display via the Options window is a different window to the Mimic Properties window that is available for individual Mimics. Although the Mimic Properties windows contain the same settings, there is a difference:

  • The Mimic Properties window displayed via the Options window has settings that apply to every new Mimic on your client PC
  • The Mimic Properties window that is displayed when you select the Properties option or command on an individual Mimic has settings that only apply to that specific Mimic.

Disclaimer

Geo SCADA Expert 2019