Configuring String Points

Add and configure an ODBC String point for each text string data value that you want to transfer between a Geo SCADA Expert system and another application, using ODBC data transfer standards.

Configure the properties of each string point using the fields on the ODBC String Point Form.

Use the fields on the ODBC tab to:

Use the fields on the Query tab to:

For information on the fields on the String Point tab, see Defining String Point Details in the Geo SCADA Expert Guide to Core Point Configuration.

For fields on other tabs on the Form, see Tabs on Point Forms in the Geo SCADA Expert Guide to Simple Drivers.


Disclaimer

Geo SCADA Expert 2019