Minimum Configuration

For an ODBC Connection to become functional (online), you need to:

You also need to put the connection In Service and save the configuration.

These are the minimum requirements and, when defined, will result in a functional connection that uses the default configuration settings.

ATTENTION: An ODBC connection can be affected by factors other than the configuration parameters within ViewX, which can cause the database to lock and stop data from being recorded


Disclaimer

Geo SCADA Expert 2019