Display the WebX Interface

ATTENTION: This topic relates to the deprecated Original WebX client that is supported by this and previous versions of Geo SCADA Expert. For information about the Virtual ViewX client that is supported by Geo SCADA Expert 2019 onwards, for which the web server is hosted using IIS, click here.

To display the WebX interface:

  1. Run Internet Explorer.
  2. To display the WebX interface from a Geo SCADA Expert server, enter http://localhost in the Address field.

    To display the WebX interface from a client, enter the server name in the Address field.

  3. Press the Enter key. This displays the WebX home page.

    If the WebX home page is not displayed, there may be a certificate error. You may need to use an alternative address or port number. For more information, see Run a Virtual ViewX Client in the Geo SCADA Expert Guide to ViewX and Virtual ViewX Clients.

The WebX home page contains a navigation bar featuring the following buttons:

When you have displayed the WebX home page, proceed to Log on to the System via WebX.

Further Information

Understand WebX: see Original WebX Client in the Geo SCADA Expert Guide to ViewX and Virtual ViewX Clients.


Disclaimer

Geo SCADA Expert 2019