Configure a TAP Pager Service

If your pager or mobile telephone provider uses a TAP interface to send messages, you will need to configure TAP Pager Service database items to represent the TAP protocol.

You need to configure one TAP Pager Service for each service provider through which you wish to send messages. For example, in the UK, to send messages through the Vodafone and Orange networks, you would need to configure two TAP Pager Services, one for the Vodafone network and one for the Orange network.

With TAP Pager Services (and UCP Pager Services), you can use multiple channels for redundancy. For example, two Pager Channels could be assigned to the same TAP Pager Service, with one channel acting as a back-up channel in case of difficulties connecting via the other channel. However, each Pager Channel can only be assigned to one Pager Service.

To configure a TAP Pager Service:

  1. Log on to your system via a User Account that has the Configure Database permission (see Allocating Security Permissions in the Geo SCADA Expert Guide to Security).
  2. Display the Pager Service Form for the Pager Service item you want to configure. If the item does not already exist in the database, you will need to Create a Pager Service Database Item.
  3. Configure the properties on the Identification, User Methods, Alarm, and Redirection tabs as required (see Tabs on Configuration Forms).
  4. Select the TAP Service tab.
  5. Configure the 'common' Pager Service properties on the tab (see Configure the Common Pager Service Properties).
  6. Configure these TAP-specific properties on the tab:
  7. Save the configuration (see Saving Configuration Changes in the Geo SCADA Expert Guide to Core Configuration).

Further Information

Configuring a Pager Channel.


Disclaimer

Geo SCADA Expert 2019