Configure the Common Channel Properties for a Pager Channel

Pager Channels have a Channel tab on their configuration Form. The Channel tab contains a variety of properties, some of which are exclusive to a particular type of Pager Channel and some of which are common to multiple types of Pager Channel.

The properties that are common to multiple types of Pager Channel include:

For information on the properties that are specific to a particular type of Pager Channel, please refer to the relevant section:


Disclaimer

Geo SCADA Expert 2019