Pager Specific Alarm and Event Categories

Each alarm and event on a Geo SCADA Expert system has a Category that indicates the type of alarm or event. The Category is included in the Events List by default and, if applicable, is also included in the Alarms List and the Alarm Banner.

If required, you can filter the entries in the Events List or Alarms List by category. You can choose to filter the lists by a variety of ‘core’ categories as well as any categories that are specific to the drivers that are installed on your system.

On systems that have the Pager driver components installed, the ‘core’ alarm and event categories are available as well as these Pager-specific categories:

Further Information

Filter Categories: see Filter a List in the Geo SCADA Expert Guide to Alarms.

Alarm Banner: see Alarm Banner in the Geo SCADA Expert Guide to Alarms.

Alarms Lists: see Alarms Lists in the Geo SCADA Expert Guide to Alarms.

Events List: see Events Lists in the Geo SCADA Expert Guide to Lists.


Disclaimer

Geo SCADA Expert 2019