SMS Messages Rejected by Geo SCADA Expert

If you send an SMS command that is rejected by Geo SCADA Expert, an alarm is raised. The alarm Message contains a description of the reason for rejecting the SMS command, which includes:

Failed to process incoming SMS command

The severity of this alarm is configured on the SMS Service object’s form (see Define whether an SMS Service can Process Incoming Messages). If this is set to ‘None’ then no alarms will be raised.

If an alarm Message includes 'SMS command rejected by Pager Driver', the SMS command has been rejected because it did not contain the required components for a valid SMS message. For more information, see SMS Messages Rejected by the Pager Driver.

There are several possible reasons for Geo SCADA Expert to reject an SMS command:


Disclaimer

Geo SCADA Expert 2019