Connect QueryPad to a Database

Before you can use QueryPad to test a query, you need to connect it to the appropriate system (the system that contains the tables that you reference in your query). QueryPad can connect to 1 system at a time.

Access to QueryPad might be restricted on your system. In order to connect QueryPad to a database successfully, the Geo SCADA Expert server has to be configured to allow SQL queries to be edited from its clients, and your User Account has to be configured to allow you to edit SQL queries. For more information, see Specify Whether SQL Queries can be Edited using the Clients on this Server, and see Define the SQL Editing Settings for a User.

To connect QueryPad to the appropriate database, you can either:


Disclaimer

Geo SCADA Expert 2019