Driver Task – Server Status Tool

The driver task contained in DriverROCPlus.exe is the program that actually communicates with the ROC. The task is under the control of Geo SCADA Expert. After you have created at least one ROC Plus object in your database, Geo SCADA Expert will automatically start the driver task. The driver task will start communicating with the ROC and undertake whatever actions it has been tasked to do.

You can check the status of the driver task by accessing the Geo SCADA Expert Server Status tool, expanding the General branch and then selecting the Modules entry.

You can right-click on the RocPlusDriver entry to display a context-sensitive menu. The menu includes options to start or stop the driver, and view the driver log file. You are unlikely to need to change the logging options from the defaults, but the driver log file is important for debugging driver problems.


Disclaimer

Geo SCADA Expert 2019