Specify the GSM Modem's Receiving Data SMS Messages Options

Use the GSM Modems Receiving Data SMS Messages section on the SCADAPack 50 tab to specify the destination and type of the SMS messages sent by the device.

NOTICE

LOSS OF DATA

To help to prevent loss of data, you need to enter the correct information in the fields on this Form.
Failure to follow these instructions can result in loss of data.

NOTICE

INOPERABLE DEVICE

Avoid leaving every Channel and every Telephone Number field blank. If you do, and you send such a configuration to the device, Geo SCADA Expert will no longer be able to communicate with the device.
Failure to follow these instructions could critically affect the operation of the device. To restore operation, a site visit may be necessary.

Disclaimer

Geo SCADA Expert 2019