Application Identifier

Associated with: Realflo controllers that are running Realflo 6.70 or later

This attribute identifies the Realflo application that is currently running in the controller.

Application identifiers are supported by Realflo version 6.70 onwards. The attribute is not displayed for controllers running versions of Realflo in which the application identifier is undefined.

Example:

SCADAPack 350 Telepace


Disclaimer

Geo SCADA Expert 2019