IP Units

IP units are used for gas flow runs. The Units column shows the measurement units. The Realflo Display column shows how these units are displayed on the screen and in printed reports.

Parameters and Values Units Realflo Display
Pipe and Orifice Diameters feet ft
Static, Base and Atmospheric Pressure lbf/ft2 lbf/ft2
Differential Pressure lbf/ft2 lbf/ft2
Flowing and Base Temperature °F °F
Viscosity lbm/ft-s lbm/ft-s
Density lbm/ft3 lbm/ft3
Mass lbm lbm
Mass Flow Rate lbm/hr lbm/hr
Volume ft3 ft3
Volume Flow Rate ft3/hr ft3/hr
Heating Value BTU(60)/ft3 BTU/ft3
Energy BTU(60) BTU
Energy Flow Rate BTU(60)/hr BTU/hr
Flow Extension (Method 1) kg/m2s kg/m2s
Turbine Rate (volume) pulses/ft3 pulses/ft3
Turbine Rate (mass) pulses/lb pulses/lb
Altitude feet feet

Disclaimer

Geo SCADA Expert 2019