Meter Input Properties

The fields within this section of the Meter Input tab display those properties that are associated with measurement.

You can configure these properties directly in Geo SCADA Expert, or read the configuration into the Geo SCADA Expert database (see Configure or Read the Flow Run Configuration).

With Gas Flow Runs, properties are only displayed on the Meter Input tab if the Flow Calculation Type is set to AGA-11 (an option that is only available from Realflo version 6.95 onwards).

The availability of the remaining fields on the tab varies, depending on the Meter Input Type. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

Further Information

For more detailed information on these properties, see the documentation provided with the Realflo application.


Disclaimer

Geo SCADA Expert 2019