Pressure Compensation Properties (Liquid Flow Run)

The properties described in this topic are supported by Realflo version 6.95 onwards.

The fields within this section of the Liquid tab comprise properties that are associated with Pressure Compensation.

You can configure these properties directly in Geo SCADA Expert, or read the configuration into the Geo SCADA Expert database (see Configure or Read the Flow Run Configuration).

Further Information

For more detailed information on these properties, see the documentation provided with the Realflo application.


Disclaimer

Geo SCADA Expert 2019