Set Clock

Associated with: SCADAPack Realflo controllers

Security permission required to access this pick action: Control

Use the Set Clock pick action to manually set the clock on a Realflo-enabled SCADAPack controller, if that clock’s time has drifted significantly.

Be aware that when a controller’s clock is set using the Realflo method (as per this pick action), the controller logs an event and restarts its current Hour log.

(Geo SCADA Expert can be configured to automatically set a controller’s Realflo clock whenever the clock drifts by more than a specified amount—for more information, see Specify Whether a Set Broadcasts Set Clock Messages in the Geo SCADA Expert Guide to the Advanced Modbus Driver, and see Define the Set Clock Method in the Geo SCADA Expert Guide to the SCADAPack Modbus Driver.)


Disclaimer

Geo SCADA Expert 2019