SCADAPack x70

Configure Poll Rates for a Slave Device

This section allows you to configure the Poll Rate parameters, which depend on the Poll Type selection in the General Settings.

Enter the required interval in the OPC Time Format. You can enter the value directly in the field, or use the Interval window (accessed via the field's browse button) to specify the required value.

The following table illustrates the relationship between the Poll Type and the Poll Rate parameters:

Poll Type Poll Rate Parameter Parameter Description
Background Poll Background Poll

This defines the interval at which the SCADAPack x70 sends an integrity poll to the DNP3 Slave. This poll is delayed when the SCADAPack x70 receives an unsolicited response from the DNP3 Slave. The Background Poll time is typically set to a smaller value than the Must Poll Interval.

Default: 65 seconds

Must Poll Interval

This defines the interval at which the SCADAPack x70sends an integrity poll to the DNP3 Slave regardless of received unsolicited responses.

Default: 65 seconds

Ratio Poll Event Poll Interval

This defines the interval between event polls.

Default: 65 seconds

Integrity Poll Ratio

This ratio determines how many event polls are issued between integrity polls.

For example, if you leave the default value of 65, there will be one integrity poll for every 65 event polls.

Default: 65

Static Only Poll Poll Interval

This defines the interval between Class 0 polls.

Default: 65 seconds

Class Poll / Time & IIN
Class Poll / Time
Class 1

This defines the poll interval for the selected Event Class.

Default: 65 seconds

Class 2
Class 3
Integrity

This defines the integrity poll interval.

Default: 65 seconds


Disclaimer

Geo SCADA Expert 2019