SCADAPack x70

Configure the Properties on the NULL Tab

The configuration Forms of SCADAPack x70 DNP3 Pulse Action (NULL) items include a NULL tab. You use the tab to configure the properties that relate to the Pulse Action's single NULL action.

The Severity, Description, and Area of Interest fields are common to pulse actions on many drivers—for information, see Define the Actions that a Pulse Undertakes in the Geo SCADA Expert Guide to Core Point Configuration. Fields that are specific to SCADAPack x70 DNP3 Pulse Action (NULL) items are explained below.


Disclaimer

Geo SCADA Expert 2019