SCADAPack x70

Create an Analog Output Point

Add a SCADAPack x70 DNP3 Analog Output Point to the database. This type of database item is available from the DNP3 sub-branch within the SCADAPack x70 branch of the Create New menu. The sub-branch corresponds to the communications protocol that Geo SCADA Expert is to use to communicate with the SCADAPack 575.

When you create the point, you can leave most of the configuration fields at their default values.

On the Analog Point tab of the configuration Form, the only fields that you need to change for this tutorial are:

Save the configuration. Notice that the DNP3 Point Number field is populated with the value that you specified for the corresponding field on the SCADAPack x70 Analog Configuration item that you referenced above.

On the Control tab, specify the following:

On the Historic tab:

Once you have configured the analog output point, you can proceed to Create an I/O Module.

Further Information

For further information about configuring a SCADAPack x70 DNP3 Analog Output Point, see Configure Analog Points for DNP3 Communications.


Disclaimer

Geo SCADA Expert 2019