SCADAPack x70

Device Configuration Serial Port Tabs

The device configuration item allows you to configure up to 4 serial ports. Each Port tab allows you to select a Port Function, which determines the configuration sections that are displayed for each function.

The following table details the Port functions and lists the associated Port Modes that can be configured for each port function.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

Port Functions Port Modes -
Serial Tabs 1 and 2
Port Modes -
Serial Tabs 3 and 4
DNP3

RS232 (RTS Off)

RS232 (RTS On)

RS232 (RTS Keyed)

Dialup Modem

RS232

RS485 2 wire

Command Line

RS232 (RTS Off)

RS232 (RTS On)

RS232

COM User(Function Block)

RS232 (RTS Off)

RS232 (RTS On)

RS232 (RTS Keyed)

RS232

RS485 2 wire

PPP/TCPIP

RS232 (RTS On)

PPP Modem

This port function is not available for Ports 3 and 4.

Terminal Server

RS232 (RTS Off)

RS232 (RTS On)

RS232 (RTS Keyed)

RS232

RS485 2 wire

Modbus

RS232 (RTS Off)

RS232 (RTS On)

RS232 (RTS Keyed)

RS232

RS485 2 wire


Disclaimer

Geo SCADA Expert 2019