SCADAPack x70

Display Configuration Download Logs

Associated with: SCADAPack x70 DNP3 outstations

Security permission required to access this pick action: Configure

A SCADAPack x70 DNP3 outstation automatically generates a log file whenever the configuration of the outstation is downloaded by Geo SCADA Expert. In addition to checking the entries in the Event Journal, you can view the raw log file to diagnose download problems.

When you download a configuration file to a SCADAPack x70 DNP3 outstation the Display Configuration Download Logs pick action is accessible from the context-sensitive menu for the outstation.

If only one log file exists then the log file is displayed directly in the Document window.

If more than one log file exists then a document window displays a list of available log files.

Select the log file you require and select Open to view the log file in a document window.


Disclaimer

Geo SCADA Expert 2019