SCADAPack x70

Security Description

Associated with: SCADAPack x70 Security Configuration items.

This status attribute indicates the Description that was entered for the .rtk file when it was imported into the Geo SCADA Expert database (see Import Security Configuration).

This attribute is only displayed if the Import Security Configuration pick action has been used to successfully import a security configuration file from the Security Adiministrator software.

Use this status attribute in conjunction with the Security File status attribute to ascertain information about the .rtk file that was imported into the Security configuration Item.


Disclaimer

Geo SCADA Expert 2019