SCADAPack x70

Setup the Active Deadband

Use this section to enable the Active Deadband Timer to delay the creation of DNP3 events. When this checkbox is selected, an Active Deadband Timer delays the creation of DNP3 events and withholds the relevant data from Class 0 poll responses. When this option is not selected, an active deadband only delays the creation of DNP3 events.

This checkbox applies to all objects that have deadbands configured.


Disclaimer

Geo SCADA Expert 2019