SCADAPack x70

Specify any Periodic Event Generation Requirements

The SCADAPack x70 tab on the Forms of SCADAPack x70 Analog and Counter Configuration items contains a Periodic Event Generation section. Use the section to specify whether the SCADAPack x70 device is to generate and store events for point data at regular intervals, in addition to generating and storing events, for example, for a change of value or state. For more information about the feature, see Periodic Event Generation.

The Periodic Event Generation section includes these properties:

 

To generate an event every 15 minutes, from 5 minutes past the hour:

Rate: 15M

Offset: 5M

The same configuration for a Counter for which the value is to be reset once an hour:

Rate: 15M

Offset: 5M

Reset Period: 1H


Disclaimer

Geo SCADA Expert 2019