SCADAPack x70

UpdateIPRowDetails

Associated with: SCADAPack x70 IP Routing Tables (on SCADAPack x70 Device Configuration items)

Security permission required to access this method: Configure

This method is the equivalent of updating the row properties within ViewX see Add and Configure the Entries in an IP Routing Table

Use these arguments for updating a row in a IP Routing table (for further information, see Using an IP Routing Table to Route TCP/IP Packets to another TCP/IP Host):


Disclaimer

Geo SCADA Expert 2019