Configuring SE RPC Analog Input Points

With Geo SCADA Expert’s SE RPC driver, you use:

You configure the properties of each SE RPC Analog Input point using fields on the SE RPC Analog Input Point Form.

This section covers configuration of properties on the Analog Point tab of the SE RPC Analog Input Point Form. For information on the fields on other tabs, see Tabs on Point Forms in the Geo SCADA Expert Guide to Advanced Drivers.

For SE RPC Analog Input points, use the Analog Point tab to:


Disclaimer

Geo SCADA Expert 2019