Define the SNMP Engine Settings

If you intend to handle inform requests from SNMP v3 devices you must configure the Boot Count and Local Engine ID for the local SNMP engine.

To perform an SNMPv3 inform request from an RTU to the SNMP driver, you need to define the Local Engine ID and engine Boot Count in the SNMP Manager section of the Geo SCADA Expert Server Configuration tool. An RTU can only talk to SNMP driver and send SNMPv3 inform request if these values are defined.

To confirm the field values select the OK button. The Local Engine ID is generated and appears in the Local Engine ID field.

Further Information

For more relating to an SNMP engine's unique identifier refer to RFC 3411 Architecture for SNMP Management Frameworks.


Disclaimer

Geo SCADA Expert 2019